You are here: Home / News / The latest news / MASI68
THE LATEST NEWS

Cube67+ More Options, More Flexible, More Profitable

February 02, 2010

Murrelektronik's Cube67 bus node provides even more flexibility in decentralized installation. Up to two times 32 modules can be connected to one bus node. In addition, Cube67+ offers the possibility of Machine Option Management.

Differing software versions and documentations for different machines are annoying for every standard machine manufacturer. Wouldn't it be useful to have only one software and one documentation to maintain? This is now possible with the Cube67+ Machine Option Management. Now create one configuration that maps the full configuration of the machine for all hardware versions. Depending on which Cube67 modules are required for the respective machine, they can be conveniently activated or deactivated either from the control panel or from the operation panel.

Murrelektronik expands its reliable Cube67 system with the innovative bus node and Machine Option Management is only one of the many benefits Cube67+ offers. It allows even greater optimization for fieldbus installations, whatever the application. Up to two times 32 modules can be connected to just one bus node.  Installations can cover long distances: cable lengths of up to two times 30 meters can be implemented. The Cube67 modules can be installed at any position along the hybrid cable and the energy supply can simply be daisy chained at the bus node.