You are here: Home / News / The latest news
THE LATEST NEWS

Cube67+ is an added PLUS for more flexibility

March 30, 2009

More modules, longer cables, increased performance: these are the outstanding features of the new innovative bus node Cube67+. It perfectly complements the tried and tested Cube67 system. With Cube67+ , Murrelektronik offers customers even more options for creating fieldbus installations in a very economical manner.

Cube67 wins over customers with its modular and flexible structure. This product line offers a wide number of various modules in which the ports are designed for multifunctional use and are available with M8 and M12 connection. All these features can create installations that solve the most special of needs. Because of this and the many diagnostic options provided, the Cube67 system has become a reputed symbol of cost savings in field installation.

With Cube67+ , Murrelektronik now offers customers many additional advantages.

The heart of this innovation is a modified bus node where up to two times 10 modules can be connected. This provides a significant advantage and enables control of almost twice as many signals and actuators. Now it is possible to considerably reduce the number of bus nodes in comprehensive installations helping to save costs.

Cube67+ can also create installations over even longer distances. So far, cable lengths of four times 10 meters have been possible. Now, with Cube67+, this has been increased to up to two times 30 meters which is very useful for C-track applications. With Cube67+, engineers can connect the modules at any position along the system cable which provides added flexibility.

Last but not least, another advantage is that the new Cube67+ bus node can connect additional modules with extended functionalities for IO link or RS232.